Coldfire: Flash programming and debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Coldfire: Flash programming and debugger

2,688 次查看
jixiang
Contributor I
Hello,
 
we are using CodeWarrior 6.3 amd M52223 controller for the application. Because the code size is big, we have to use Flash programmer. Can we use debugger to debug the program?
 
Thank you,
 
dong Sun

Message Edited by CrasyCat on 2007-04-13 01:21 PM

Message Edited by CrasyCat on 2007-04-13 01:21 PM

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,307 次查看
CrasyCat
Specialist III
Hello
 
This should work.
I know there is a limitation in the number of breakpoints you can use while debugging an application in Flash. Number of breakpoints you can set in flash is limited by the number of hardware breakpoints available on the hardware.
 
 
CrasyCat
0 项奖励
回复

1,307 次查看
Nouchi
Senior Contributor II
Hello,

3 PC breakpoints maximum, see MCF52223RM Rev2 chapter 27 (debug module)

regards,
Emmanuel
0 项奖励
回复