Coldfire: Flash programming and debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire: Flash programming and debugger

2,745件の閲覧回数
jixiang
Contributor I
Hello,
 
we are using CodeWarrior 6.3 amd M52223 controller for the application. Because the code size is big, we have to use Flash programmer. Can we use debugger to debug the program?
 
Thank you,
 
dong Sun

Message Edited by CrasyCat on 2007-04-13 01:21 PM

Message Edited by CrasyCat on 2007-04-13 01:21 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,364件の閲覧回数
CrasyCat
Specialist III
Hello
 
This should work.
I know there is a limitation in the number of breakpoints you can use while debugging an application in Flash. Number of breakpoints you can set in flash is limited by the number of hardware breakpoints available on the hardware.
 
 
CrasyCat
0 件の賞賛
返信

1,364件の閲覧回数
Nouchi
Senior Contributor II
Hello,

3 PC breakpoints maximum, see MCF52223RM Rev2 chapter 27 (debug module)

regards,
Emmanuel
0 件の賞賛
返信