CodeWarrior cannot connect to CWTAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior cannot connect to CWTAP

Jump to solution
5,108 Views
Bandar
Contributor IV

Hello everyone,

I’m reaching out after spending several days attempting to bring up the CodeWarrior TAP with the FRWY-LS1046AGSG board for initial debug and SerDes configuration using QCVS. I have a strong embedded background and carefully verified all configuration steps, but my PCs failed to connect to CWTAP and fails to detect the target SoC.

Setup:

  • Board: FRWY-LS1046AGSG

  • CW TAP Kit:

    • CWH-CTP-BASE-HE

    • CWH-CTP-CTX10-YE

     

  • Connections -different PC/OS-:

    • PC (Windows 10 / Windows 11 / Linux) ↔ Ethernet/USB ↔ CWTAP ↔ JTAG ↔ LS1046

     

  • Software: CW4NET v2020.06, QCVS, CCS

What works:

  • CW TAP was configured via serial console (see screenshot below).

Burses_5-1747602451845.png

  • CWTAP and PC can ping each other.

  • I can run the following and get version response from CW TAP:

Burses_6-1747602499857.png

  • findcc discovers the TAP ( I've connected the USB and the Eth).

Burses_9-1747605804653.png

 

What fails:

 

cannot find the CWTAP USB 

Burses_7-1747602563105.png

QCVS SerDes Configuration Tool Failed:

Burses_8-1747602591956.png

  • Target is powered, not held in reset, and run the default QSPI and tried to run the SD Card that comes with FREEWAY board which contains ubuntu 18. ( I interrupt u-boot)

Closest issue I found (but unresolved):

https://community.nxp.com/t5/PowerQUICC-Processors/CWTAP-is-not-found-from-CW-connections-view/m-p/1...

 

Thanks in advance.

0 Kudos
Reply
1 Solution
4,945 Views
Bandar
Contributor IV

Dear June thanks for your support I identified the main issue is the update, once I try to apply update as you mentioned or from online
I got this error

Burses_2-1747857190258.png

and if this error for some reasons the Target connections is dispersed and show an error once it been loaded 

so the area in red is showing no devices 

Burses_1-1747857169342.png

so I decide to skip the update and just install it the executable file and everything works fine

Burses_3-1747857243954.png

 

Thanks again!

View solution in original post

0 Kudos
Reply
11 Replies
5,055 Views
June_Lu
NXP TechSupport
NXP TechSupport

It seems idcode.tcl works well.

Try the command below:

ccs::config_chain{ ls1043a dap sap2}

display ::ccs::get_config_chain

Thanks

0 Kudos
Reply
5,036 Views
Bandar
Contributor IV

Please find the results here

 

Burses_0-1747668622084.png

 

 

this is the output of u-boot from freeway dev board

Burses_1-1747668642543.png

 

 

but still I cannot connect from cw ! 

Burses_2-1747668766792.png

 

0 Kudos
Reply
5,055 Views
June_Lu
NXP TechSupport
NXP TechSupport

Is the FRWY-LS1046A could bring up with logs output?

Have you every linked the CWTAP with the ethernet?

0 Kudos
Reply
5,034 Views
Bandar
Contributor IV
FRWY-LS1046A shows the output logs and shared in screenshot above.

This is my first time using CWTAP.
0 Kudos
Reply
5,012 Views
June_Lu
NXP TechSupport
NXP TechSupport

CCS could connect the FRWY-LS1046A.

"duplicate" FRWY-LS1046A in the CodeWarrior(CW) IDE, set the "Target Configuration" with your Ethernet IP, run "Diagnose", if it passed, CW IDE works well.

How about your CodeWarrior(CW) IDE license?

https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools...

Developer Suite Level

Specialist Suite Level

Only "Specialist Suite Level" could support DDR QCVS.

0 Kudos
Reply
5,000 Views
Bandar
Contributor IV

This is my CW version, and for now I'm using the evaluation license 

Burses_0-1747725370847.png

Burses_1-1747725376026.png

Regarding the Diagnostic, I opened the Target Connections Windows and try to add Board but it give me error

"Could not create new configuration due to start up errors.
Could not load internal database, path is invalid: C:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\SoCs\gta\SoCs"

while I can see the Connection View Windows I can add my target but the connection failed

Burses_4-1747725935851.png

 

 

 

 

 

Lastly, why we chose LS1043A and LS1046A not exist in CCS?

Burses_2-1747725415686.png

while LS1043A

Burses_3-1747725439452.png

 

 

0 Kudos
Reply
4,969 Views
June_Lu
NXP TechSupport
NXP TechSupport

Could you confirm if the evaluation version is not expired? When do you download the CodeWarrior?

Please install CodeWarrior® Development Suites for Networked Applications 11.5.12 to run the QCVS DDR.

Please find link below:

https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools...

Select “DOWNLOAD EVAL”

 Download update package

com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip

 

Please open CodeWarrior from C:\Freescale\CW4NET_v2020.06\CW_ARMv8\fsl_eclipse.bat, and install the update package from Help->Install New Software->Add->Archive.

 

Please reopen CodeWarrior in a new workspace.

 

Please confirm the "Diagnose" works well, please follow C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual, 5.1 Target Connection configurator overview

"duplicate" FRWY-LS1046A in the CodeWarrior(CW) IDE, set the "Target Configuration" with your Ethernet IP, run "Diagnose", if it passed, CW IDE works well.

 

If it could not work correctly please reinstall the CodeWarrior again.

 

After confirm above, try the QCVS again.

Please use "ccs::config_chain{ ls1043a dap sap2}" to connect LS1046A, any other command is not available.

0 Kudos
Reply
4,946 Views
Bandar
Contributor IV

Dear June thanks for your support I identified the main issue is the update, once I try to apply update as you mentioned or from online
I got this error

Burses_2-1747857190258.png

and if this error for some reasons the Target connections is dispersed and show an error once it been loaded 

so the area in red is showing no devices 

Burses_1-1747857169342.png

so I decide to skip the update and just install it the executable file and everything works fine

Burses_3-1747857243954.png

 

Thanks again!

0 Kudos
Reply
5,082 Views
June_Lu
NXP TechSupport
NXP TechSupport

Would your board in hand is FRWY-LS1046A(LS1046A Freeway Board) or customer board but designed based on the FRWY-LS1046A?

Thanks

0 Kudos
Reply
5,069 Views
Bandar
Contributor IV
Hi June, it's the dev board FRWY-LS1046A
0 Kudos
Reply
5,102 Views
Bandar
Contributor IV

if I source IDcode.tcl It confirms the setup is properly set

Burses_0-1747608261109.png

 

0 Kudos
Reply