CodeWarrior TAP red light problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior TAP red light problem

ソリューションへジャンプ
3,986件の閲覧回数
PaulWalker
Contributor IV

Re: CodeWarrior TAP, CWH-CTP-BASE-HE

 

Plugging in TAP via USB or Ethernet (with USB power), TAP always has solid RED light.

Is the TAP broken, or can it be recovered?

I have 2 out of 4 TAP's doing this now, which have mostly just been sitting on a bench, plugged in.

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,619件の閲覧回数
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,617件の閲覧回数
hwrobel
NXP Employee
NXP Employee

You may want to contact your friendly Freescale support.

I assume that the TAP no longer enumerates as USB device under Windows.

Assuming that the TAP HW is still ok, this would indicate loss of the firmware for TBD reasons.

In that case, recovery is possible, but it requires opening the tap and it requires software tools and images not available outside Freescale.

There is nothing that can be done here on the Forum.

3,620件の閲覧回数
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

0 件の賞賛
返信
3,617件の閲覧回数
PaulWalker
Contributor IV

Extra info that might be relevent:

CodeWarrior Basic Edition, 10.3.3

TAP has markings:

900-76173

REV-B

13172206

CodeWarrior TAP console COM port does not appear in device manager - so cannot query for ccs info