CodeWarrior TAP red light problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior TAP red light problem

Jump to solution
4,004 Views
PaulWalker
Contributor IV

Re: CodeWarrior TAP, CWH-CTP-BASE-HE

 

Plugging in TAP via USB or Ethernet (with USB power), TAP always has solid RED light.

Is the TAP broken, or can it be recovered?

I have 2 out of 4 TAP's doing this now, which have mostly just been sitting on a bench, plugged in.

 

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,637 Views
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

View solution in original post

0 Kudos
Reply
3 Replies
3,635 Views
hwrobel
NXP Employee
NXP Employee

You may want to contact your friendly Freescale support.

I assume that the TAP no longer enumerates as USB device under Windows.

Assuming that the TAP HW is still ok, this would indicate loss of the firmware for TBD reasons.

In that case, recovery is possible, but it requires opening the tap and it requires software tools and images not available outside Freescale.

There is nothing that can be done here on the Forum.

3,638 Views
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

0 Kudos
Reply
3,635 Views
PaulWalker
Contributor IV

Extra info that might be relevent:

CodeWarrior Basic Edition, 10.3.3

TAP has markings:

900-76173

REV-B

13172206

CodeWarrior TAP console COM port does not appear in device manager - so cannot query for ccs info