CodeWarrior TAP red light problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior TAP red light problem

跳至解决方案
3,994 次查看
PaulWalker
Contributor IV

Re: CodeWarrior TAP, CWH-CTP-BASE-HE

 

Plugging in TAP via USB or Ethernet (with USB power), TAP always has solid RED light.

Is the TAP broken, or can it be recovered?

I have 2 out of 4 TAP's doing this now, which have mostly just been sitting on a bench, plugged in.

 

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,627 次查看
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,625 次查看
hwrobel
NXP Employee
NXP Employee

You may want to contact your friendly Freescale support.

I assume that the TAP no longer enumerates as USB device under Windows.

Assuming that the TAP HW is still ok, this would indicate loss of the firmware for TBD reasons.

In that case, recovery is possible, but it requires opening the tap and it requires software tools and images not available outside Freescale.

There is nothing that can be done here on the Forum.

3,628 次查看
PaulWalker
Contributor IV

Thanks for help. I have contacted my local Freescale rep for help.

0 项奖励
回复
3,625 次查看
PaulWalker
Contributor IV

Extra info that might be relevent:

CodeWarrior Basic Edition, 10.3.3

TAP has markings:

900-76173

REV-B

13172206

CodeWarrior TAP console COM port does not appear in device manager - so cannot query for ccs info