why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

ソリューションへジャンプ
2,005件の閲覧回数
KingZhang
Contributor I
why my codewarrior HCS08 5.1  create a new project or click open project button ,will close the codewarrior window?but no this problem on my notebook .
 
I think the codewarrior if ready to using "open folder" or "create file or folder" window ,this problem will appear.
 
my computer operating system is Windows XP SP2.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,014件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,015件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel
0 件の賞賛
返信
1,014件の閲覧回数
KingZhang
Contributor I
Hi,CompilerGuru
 
I'm Uncheck "Run this program in compatibility mode for". it works beautifully.
 
Thanks your help,
 

 
0 件の賞賛
返信