where is MCUinit.c in Codewarrior 10.5 for kinetis L?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is MCUinit.c in Codewarrior 10.5 for kinetis L?

1,349件の閲覧回数
stefanomanca
Contributor III

Hi, in codewarrior 10.3 I had the chance to create a new bare project using the device initialization feature and codewarrior generated the MCUinit.c.

How can I do the same in codewarrior 10.5?

 

Thank you.

 

Stefano M.

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

1,165件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

in CW10.5, please select "hardware configuration (pin muxing and device initialization)" when creating a new project:

untitled.JPG.jpg

0 件の賞賛
返信

1,165件の閲覧回数
stefanomanca
Contributor III

My needs are only having the clock registers initialized and the rest done by hand. I want to add a interrupt isr by hand but every time i do "generate processor expert code" it deletes my isr name from vector table in cpu.c file. How can solve it? By CW 10.3 it was easy, I generated once MCUinit.c then I choose "create file and do not add to the project" in "device initialization project options" menu.

Hon can solve it?

Thank you.

0 件の賞賛
返信

1,165件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

"Device Initialization" option was removed from CW V10.5. However in case you select PEx options you should almost the same project, functionality, etc,... In case you need to add your own vector to Vectors.c please use InterruptVector component for this task. To show this component in Component Library is necessary to switch off the filter button (you can find more details on PEx community forum), this bug is going to be fixed in CW V10.6.

Best regards

Vojtech Filip

Processor Expert Support Team

1,165件の閲覧回数
stefanomanca
Contributor III

Hi, It doesn't generate the file MCUinit.c

0 件の賞賛
返信