How to enable Processor Expert for Relocatable Assembly in CW10.4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Processor Expert for Relocatable Assembly in CW10.4?

1,645 Views
mylim
Contributor IV

Hi, I'd like to find out how to enable Processor Expert for Relocatable Assembly in CW10.4 for MCU?

It seems like I only able to see PE with I select C when creating a project.

Please advise.

Thanks.

 

Regards,

MY

Labels (1)
0 Kudos
Reply
3 Replies

1,523 Views
trytohelp
NXP Employee
NXP Employee

Hi,

This issue was logged in our Service Request under the number 1-1263627071.

See below the Freescale  answers:

     

++++++++++++++++++

You are correct that PE option is only available after user select to create a C language project. We have no plan to support assembly project in PE. Sorry for this inconvenience.

It's same for Device Initialization, this option is only available after user select C language when creating project.

++++++++++++++++++

Regards

Pascal

0 Kudos
Reply

1,523 Views
BlackNight
NXP Employee
NXP Employee

I suggest that you create a new C project with Processor Expert, and then you simply add your assembly files to it.

That gives you everything from both world (C, relocatable assembly). You need at least some C portion as Processor Expert code is in C.

Hope this helps,

Erich

0 Kudos
Reply

1,523 Views
mylim
Contributor IV

Thanks  BlackNight

I can see that they are killing the assembler community. :smileysad:

0 Kudos
Reply