what patches need to add to work on KEA128 with LIN?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what patches need to add to work on KEA128 with LIN?

1,203 次查看
Abil
Contributor II

Hello,

Do i need to add patches to work on KEA128 or can i  directly run examples available for KE series as it is? also suggest for LIN application with KEA128 what patches do i need to add

Thanks...

标签 (1)
0 项奖励
回复
2 回复数

1,086 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi shweta karade

You don't need any patch to work with KEA128, you should be able to run examples for your device. There are available some sample codes for TRK-KEA128, you could check them and change them as you need.

For LIN application, there is a LIN stack package available that you can use with KEA, "LIN2.x and SAE J2602 Stack". I recommend you to download it and start with this.


Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,086 次查看
Abil
Contributor II

Thank you

On Wed, Aug 3, 2016 at 9:39 PM, jorge_a_vazquez <

0 项奖励
回复