using multiple ADC Bean on a MC9S08AW32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using multiple ADC Bean on a MC9S08AW32

ソリューションへジャンプ
1,772件の閲覧回数
vlm
Contributor I
Hi,
 
I'm using Processor Expert in an application based on a MC9S08AW32.
I want to use either the ADC with 6 inputs or the ADC with 2 other inputs (differents  from the 6 first), depending on a code received from the serial port.
With Processor Expert I select the ADC Bean and configure it with the 6 first channels.
Processor Expert refuse the declaration of a second ADC Bean.
Is there a way to solve this problem ?
 
Thanks,
Vincent


J2MEJediMaster added MCU to header

Message Edited by J2MEJediMaster on 2007-04-25 10:33 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
861件の閲覧回数
vlm
Contributor I
Hi,
 
I'finally found by myself : switch the item "sharing" to "enabled" for each of the ADC bean.
 
Vincent

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
862件の閲覧回数
vlm
Contributor I
Hi,
 
I'finally found by myself : switch the item "sharing" to "enabled" for each of the ADC bean.
 
Vincent
0 件の賞賛
返信