using multiple ADC Bean on a MC9S08AW32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using multiple ADC Bean on a MC9S08AW32

Jump to solution
2,450 Views
vlm
Contributor I
Hi,
 
I'm using Processor Expert in an application based on a MC9S08AW32.
I want to use either the ADC with 6 inputs or the ADC with 2 other inputs (differents  from the 6 first), depending on a code received from the serial port.
With Processor Expert I select the ADC Bean and configure it with the 6 first channels.
Processor Expert refuse the declaration of a second ADC Bean.
Is there a way to solve this problem ?
 
Thanks,
Vincent


J2MEJediMaster added MCU to header

Message Edited by J2MEJediMaster on 2007-04-25 10:33 AM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,539 Views
vlm
Contributor I
Hi,
 
I'finally found by myself : switch the item "sharing" to "enabled" for each of the ADC bean.
 
Vincent

View solution in original post

0 Kudos
Reply
1 Reply
1,540 Views
vlm
Contributor I
Hi,
 
I'finally found by myself : switch the item "sharing" to "enabled" for each of the ADC bean.
 
Vincent
0 Kudos
Reply