Trim adjust and USB Multilink Pemicro on S08AW32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trim adjust and USB Multilink Pemicro on S08AW32

ソリューションへジャンプ
2,563件の閲覧回数
PO220
Contributor IV
Hi,

I do not succeed to manage automatically the trim of my S08AW32 with the USB Multilink Pemicro.

In "BDM_P&E_Multilink_CyclonePro.ini" there is well "AUTO_SYNC=1"

and in the program there is well " ICGTRM = *(unsigned char*)0xFFBE ;" after FLL initialisation.

but It is not working....

As we can see it on the forums of www.68hc08.net, I am not the only one to have this problem.

Thank you in advance for your help

http://www.68hc08.net
La communauté francophone
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
998件の閲覧回数
peg
Senior Contributor IV
Hi,
 
Before posting, please try to search for the answers yourself.
 
Here is the post that explains this:
 
 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
999件の閲覧回数
peg
Senior Contributor IV
Hi,
 
Before posting, please try to search for the answers yourself.
 
Here is the post that explains this:
 
 
0 件の賞賛
返信
998件の閲覧回数
PO220
Contributor IV

excuse me, I did not see this one...

however, an other member of www.68hc08.net found it before ! It's working very well after suppression of the comments in aw.s08p file

this new post will allow another newby to find the answer more quickly, maybe...

thank you

0 件の賞賛
返信