usbdm et code warrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

usbdm et code warrior

跳至解决方案
2,391 次查看
bourineauthierr
Contributor I

bonjour

j'ai fabriqué un programmateur usbdm

et installé usbdm version: 4.12.1.40

CodeWarrior for MCU

     Version: 10.6

     Build Id:140329

 

impossible de voir le device sous code warrior :

choix usbdm non présent lors de la création d'un nouveau projet.

 

merci de votre aide

标签 (1)
0 项奖励
回复
1 解答
2,240 次查看
pgo
Senior Contributor V

Hi Thierry,

Could I check:

  • Did you install USBDM after Codewarrior?
  • Is Codewarrior detected by the installer (it should appear selected)?
  • Does USBDM appear in the about Codewarrior dialogue?

pastedImage_4.png

  • If you click on the icon it should produce more information:

pastedImage_0.png

I confirmed that I was able to create a project for the MC9S08QD4 device with a USBDM launch configuration.

It is necessary to install USBDM after Codewarrior (and possibly re-install after a major update) as USBDM modifies the Codewarrior installation.

bye

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,240 次查看
pgo
Senior Contributor V

Hi Thierry,

Could I check:

  • Did you install USBDM after Codewarrior?
  • Is Codewarrior detected by the installer (it should appear selected)?
  • Does USBDM appear in the about Codewarrior dialogue?

pastedImage_4.png

  • If you click on the icon it should produce more information:

pastedImage_0.png

I confirmed that I was able to create a project for the MC9S08QD4 device with a USBDM launch configuration.

It is necessary to install USBDM after Codewarrior (and possibly re-install after a major update) as USBDM modifies the Codewarrior installation.

bye

0 项奖励
回复
2,240 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Thierry

What is the part number of your MCU?

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 项奖励
回复
2,240 次查看
bourineauthierr
Contributor I

Hi,

The part as target is  s9s08QD4

The part usbdm is s9s08js16CWJ

I checked each connection of the PCB ..I

Code warrior is a special edition.

I will deinstall and reinstall code warrior  and to check again

Thank

0 项奖励
回复