problem installing code warrior for hc08- V5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem installing code warrior for hc08- V5.1

Jump to solution
3,398 Views
venki
Contributor I

Dear Sir,

not able to install code warrior for HC-08-V5.1 with windows-vista platform

 

below are errors during Installation.

Unknown error occured during the license file copy process.Please copy the license.dat file manualy from \setup1\disk1 to your target directory.

Failed to install windriver's Kernel Module.Error creating device info element.Access is denied.

Failed tring to install the driver.

Error 1722

There is a problem with this windows installer Package.

A program run as part of the setup did not finish as expected.Contact your Support Personnel or package vendor

Rolling back action

 

 

Best Regards

Venki

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,435 Views
peg
Senior Contributor IV
0 Kudos
Reply
1 Reply
1,436 Views
peg
Senior Contributor IV
Hi Venki,
 
Please refer to this answer by the Codewarrior Guru, CrasyCat.
 
 
0 Kudos
Reply