problem installing code warrior for hc08- V5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem installing code warrior for hc08- V5.1

ソリューションへジャンプ
3,436件の閲覧回数
venki
Contributor I

Dear Sir,

not able to install code warrior for HC-08-V5.1 with windows-vista platform

 

below are errors during Installation.

Unknown error occured during the license file copy process.Please copy the license.dat file manualy from \setup1\disk1 to your target directory.

Failed to install windriver's Kernel Module.Error creating device info element.Access is denied.

Failed tring to install the driver.

Error 1722

There is a problem with this windows installer Package.

A program run as part of the setup did not finish as expected.Contact your Support Personnel or package vendor

Rolling back action

 

 

Best Regards

Venki

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,473件の閲覧回数
peg
Senior Contributor IV
0 件の賞賛
返信
1 返信
1,474件の閲覧回数
peg
Senior Contributor IV
Hi Venki,
 
Please refer to this answer by the Codewarrior Guru, CrasyCat.
 
 
0 件の賞賛
返信