Sharing CWS4.5 (for HCS12X) with 2 dongles for 3 users

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sharing CWS4.5 (for HCS12X) with 2 dongles for 3 users

Jump to solution
1,994 Views
MickLauffer
Contributor I
Hi

We plan to upgrade our 2 existing CodeWarrior licenses (v3.1 for HC12S) to the newest version (4.5 for HCS12S).
So far we worked with licenses tied to the hardware-ID but now we plan to buy USB dongles in order that more than 2 people may share those two licenses. Will it work like that, e.g. that those 2 dongles are used on 3 different PCs (in different combinations) or is it like that one PC works only with a dedicated dongle (which may be shared for different PCs)? Or in different words: does it matter which dongle is attached to the PC or is it possible to have a "pool" of dongles for different PCs?

TIA,
Mick

Message Edited by Mick Lauffer on 2007-04-1611:35 AM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,289 Views
Alban
Senior Contributor II
Hello Tom & Mick,

licensing@metrowerks.com seems not to be transferred to @freescale.com (not in the list)

Emails to license@freescale.com are received for sure.

The other option is always to create a Service Request :smileyhappy:

Cheers,
Alban.


View solution in original post

0 Kudos
Reply
2 Replies
1,289 Views
J2MEJediMaster
Specialist I
I think you can share the dongles around, but check this forum thread. E-mail licensing@freescale.com for a definitive answer.

---Tom
1,290 Views
Alban
Senior Contributor II
Hello Tom & Mick,

licensing@metrowerks.com seems not to be transferred to @freescale.com (not in the list)

Emails to license@freescale.com are received for sure.

The other option is always to create a Service Request :smileyhappy:

Cheers,
Alban.


0 Kudos
Reply