Which OS runs Codewarrier for 9S12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which OS runs Codewarrier for 9S12

ソリューションへジャンプ
1,398件の閲覧回数
jcdammeyer
Contributor III

Last year I did a major project using a 9S12. 

 

My verison of CodeWarrier is CodeWarrier Development Studio for HC12 4.7.1 Patch build 8204 IDE Version 5.9 which was only supported under Win-XP and not VISTA.

 

I may have to do some major updates to the project but the development environment will more than likely be Win7.  What's the status with regards to Win7 64 bit?  From what I understand none of the debuggers that have drivers for the 32 bit WIN-XP will function in the Win7 environment.

 

I've been looking through the Freescale site for some sort of app note or white paper on this but haven't found anything.  Anyone have links to this sort of information?

 

Any suggestions for a Win7 compatible ICE type debugger?

 

Thanks

John

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,000件の閲覧回数
jcdammeyer
Contributor III

Ah.  Found it.  Seems the 5.9 IDE Rev does run under Vista.  Always happens that way.  Post a request, then find the answer.

John

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,001件の閲覧回数
jcdammeyer
Contributor III

Ah.  Found it.  Seems the 5.9 IDE Rev does run under Vista.  Always happens that way.  Post a request, then find the answer.

John

0 件の賞賛
返信