Which OS runs Codewarrier for 9S12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which OS runs Codewarrier for 9S12

跳至解决方案
1,968 次查看
jcdammeyer
Contributor III

Last year I did a major project using a 9S12. 

 

My verison of CodeWarrier is CodeWarrier Development Studio for HC12 4.7.1 Patch build 8204 IDE Version 5.9 which was only supported under Win-XP and not VISTA.

 

I may have to do some major updates to the project but the development environment will more than likely be Win7.  What's the status with regards to Win7 64 bit?  From what I understand none of the debuggers that have drivers for the 32 bit WIN-XP will function in the Win7 environment.

 

I've been looking through the Freescale site for some sort of app note or white paper on this but haven't found anything.  Anyone have links to this sort of information?

 

Any suggestions for a Win7 compatible ICE type debugger?

 

Thanks

John

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,570 次查看
jcdammeyer
Contributor III

Ah.  Found it.  Seems the 5.9 IDE Rev does run under Vista.  Always happens that way.  Post a request, then find the answer.

John

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,571 次查看
jcdammeyer
Contributor III

Ah.  Found it.  Seems the 5.9 IDE Rev does run under Vista.  Always happens that way.  Post a request, then find the answer.

John

0 项奖励
回复