What debugger command could "open configuration" in Hi-wave?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What debugger command could "open configuration" in Hi-wave?

ソリューションへジャンプ
1,484件の閲覧回数
DanielTan
Contributor I

In Hi-wave, "File->Open Configuration" could a load a .ini file.

Could I use a debugger command in Command component to load a .ini file?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
943件の閲覧回数
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
944件の閲覧回数
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

0 件の賞賛
返信