What debugger command could "open configuration" in Hi-wave?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What debugger command could "open configuration" in Hi-wave?

Jump to solution
1,481 Views
DanielTan
Contributor I

In Hi-wave, "File->Open Configuration" could a load a .ini file.

Could I use a debugger command in Command component to load a .ini file?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
940 Views
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
941 Views
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

0 Kudos
Reply