Using the Visualization Tool to generate an interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the Visualization Tool to generate an interrupt

Jump to solution
4,204 Views
whitea
Contributor I

Is there any way to use the Visualization Tool, particularily the switches, to generate an interrupt? I am currently trying to generate the IRQ_L interrupt using a switch. I understand the IRQ_L is the 2nd LSB of Port E. While I can modify this value using the switch, no interrupt occurs as far as I can tell. Any help would be greatly appreciated as the documentation on the Visualization Tool does not address interrupts. Thank you.

Andy

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,981 Views
CrasyCat
Specialist III

Hello

 

Today you cannot generate an interrupt from the visualization tool.

 

CrasyCat

View solution in original post

0 Kudos
Reply
4 Replies
2,981 Views
whitea
Contributor I
Thank you so much for the response. Is there a way to generate an interrupt using any of the components other than the IT_Keyboard? I'm still using an old version (4.6) as a teaching aid and it has the old components that version 5.0 does not.
0 Kudos
Reply
2,981 Views
whitea
Contributor I
I also meant to mention that I'm using the Simulator and Debugger and not actual hardware. Is there a way in the Simulator to generate an interrupt? (other than the IT_Keyboard component)
0 Kudos
Reply
2,981 Views
CrasyCat
Specialist III

Hello

 

Only component I know allowing you to stimulate (Raise) an interrupt is the stimulation component.

 

Bad news is that component is available in professional edition only and for HC12, HCS12 AND HCS12X MCUs only.

 

CrasyCat

2,982 Views
CrasyCat
Specialist III

Hello

 

Today you cannot generate an interrupt from the visualization tool.

 

CrasyCat

0 Kudos
Reply