Using the Visualization Tool to generate an interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the Visualization Tool to generate an interrupt

ソリューションへジャンプ
4,335件の閲覧回数
whitea
Contributor I

Is there any way to use the Visualization Tool, particularily the switches, to generate an interrupt? I am currently trying to generate the IRQ_L interrupt using a switch. I understand the IRQ_L is the 2nd LSB of Port E. While I can modify this value using the switch, no interrupt occurs as far as I can tell. Any help would be greatly appreciated as the documentation on the Visualization Tool does not address interrupts. Thank you.

Andy

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,112件の閲覧回数
CrasyCat
Specialist III

Hello

 

Today you cannot generate an interrupt from the visualization tool.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,112件の閲覧回数
whitea
Contributor I
Thank you so much for the response. Is there a way to generate an interrupt using any of the components other than the IT_Keyboard? I'm still using an old version (4.6) as a teaching aid and it has the old components that version 5.0 does not.
0 件の賞賛
返信
3,112件の閲覧回数
whitea
Contributor I
I also meant to mention that I'm using the Simulator and Debugger and not actual hardware. Is there a way in the Simulator to generate an interrupt? (other than the IT_Keyboard component)
0 件の賞賛
返信
3,112件の閲覧回数
CrasyCat
Specialist III

Hello

 

Only component I know allowing you to stimulate (Raise) an interrupt is the stimulation component.

 

Bad news is that component is available in professional edition only and for HC12, HCS12 AND HCS12X MCUs only.

 

CrasyCat

3,113件の閲覧回数
CrasyCat
Specialist III

Hello

 

Today you cannot generate an interrupt from the visualization tool.

 

CrasyCat

0 件の賞賛
返信