TX problem on MC9S08AC60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TX problem on MC9S08AC60

ソリューションへジャンプ
1,817件の閲覧回数
BagdatBaibussin
Contributor I

I have  tested SCI 2 with  debug.h on evaluation board - OK  with code Warrior

On my board T2DX problem on MC9S08AC60 - Stlll High Receiver OK

Trasmiter - High level

only one difference - Package LQFP    QFP  

HElp Me!!!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,582件の閲覧回数
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,583件の閲覧回数
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

0 件の賞賛
返信