TX problem on MC9S08AC60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TX problem on MC9S08AC60

Jump to solution
1,813 Views
BagdatBaibussin
Contributor I

I have  tested SCI 2 with  debug.h on evaluation board - OK  with code Warrior

On my board T2DX problem on MC9S08AC60 - Stlll High Receiver OK

Trasmiter - High level

only one difference - Package LQFP    QFP  

HElp Me!!!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,578 Views
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

View solution in original post

0 Kudos
Reply
1 Reply
1,579 Views
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

0 Kudos
Reply