TX problem on MC9S08AC60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TX problem on MC9S08AC60

跳至解决方案
1,815 次查看
BagdatBaibussin
Contributor I

I have  tested SCI 2 with  debug.h on evaluation board - OK  with code Warrior

On my board T2DX problem on MC9S08AC60 - Stlll High Receiver OK

Trasmiter - High level

only one difference - Package LQFP    QFP  

HElp Me!!!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,580 次查看
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,581 次查看
Jim_P
Contributor III

on the development board is there the standard RS232 driver - - - it inverts.

 

on your board did you directly connect the pin to the connector if so - - - check the settings for the SCI,  and have the transmitter inverted - - - might need to do the same with the receiver setting.

 

I direct connect and invert both of these settings. - - - -  Development board allows for providing and handling full RS232 levels.

 

Jim P

0 项奖励
回复