Stop Pop Up at startup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stop Pop Up at startup

Jump to solution
2,029 Views
ronaldpatton
Contributor I

Hi,

 

How do I prevent this pop up when starting Code Warrior 10.6?  The evaluation version was initially installed.  It has since auto down graded to the "community version".

 

71753_71753.jpgScreenshot 2015-09-04 11.02.14_cr.jpg

Regards,

Ron

Labels (1)
0 Kudos
Reply
1 Solution
1,896 Views
BlackNight
NXP Employee
NXP Employee

Hi Ron,

Simply rename the file <install>\MCU\license.dat to a different name so it is not found.

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
1,897 Views
BlackNight
NXP Employee
NXP Employee

Hi Ron,

Simply rename the file <install>\MCU\license.dat to a different name so it is not found.

I hope this helps,

Erich

0 Kudos
Reply
1,896 Views
ronaldpatton
Contributor I

Yes, that did the trick,  thanks !

0 Kudos
Reply