Stop Pop Up at startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stop Pop Up at startup

ソリューションへジャンプ
2,022件の閲覧回数
ronaldpatton
Contributor I

Hi,

 

How do I prevent this pop up when starting Code Warrior 10.6?  The evaluation version was initially installed.  It has since auto down graded to the "community version".

 

71753_71753.jpgScreenshot 2015-09-04 11.02.14_cr.jpg

Regards,

Ron

ラベル(1)
0 件の賞賛
返信
1 解決策
1,889件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ron,

Simply rename the file <install>\MCU\license.dat to a different name so it is not found.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,890件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ron,

Simply rename the file <install>\MCU\license.dat to a different name so it is not found.

I hope this helps,

Erich

0 件の賞賛
返信
1,889件の閲覧回数
ronaldpatton
Contributor I

Yes, that did the trick,  thanks !

0 件の賞賛
返信