Source Code is Missing on degugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source Code is Missing on degugging

Jump to solution
1,799 Views
hitoshihosaka
Contributor I

Hi All,

My configuration with Code Warrior 10 has problem.

Before I knew it, My configuration is missing source code for a project. it alway say "No Source available for XX".

I can create break point on a source code, it looks work fine, Disassembly window show correct part,  valiables shows correct values, just source code does not show it.

I have confirmed debug configuration>source. there is default, it includes target project folder.

I have compared coworkers it handles same project. I cannot any defference with these settings but it works well, not same as mine.

I have also tried to uninstall / install Code Warrior, Create new workspace with new project. it meaning there are no .metadata or .setting. but still my configuration cannot find source files.

 

Would you like to give me any suggestion for me?

 

Thank you

Labels (1)
0 Kudos
Reply
1 Solution
1,672 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hitoshi,

Which version Code Warrior do you used ? CW10.6 CW 10.5 or anything else ?

Which chip do you used ?

And have you test create one simple project ,then  build , debug ?

You said when debug it shows  "No Source available for XX". do you meaning

when build it have no error ?

You can take a screenshot about the error and your steps.

Hope it helps

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,672 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hitoshi,

Which version Code Warrior do you used ? CW10.6 CW 10.5 or anything else ?

Which chip do you used ?

And have you test create one simple project ,then  build , debug ?

You said when debug it shows  "No Source available for XX". do you meaning

when build it have no error ?

You can take a screenshot about the error and your steps.

Hope it helps

Alice

0 Kudos
Reply