Software tool for KW20 Family MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software tool for KW20 Family MCU

ソリューションへジャンプ
2,299件の閲覧回数
admin
Specialist II

The  KW20 MCU (Cortex4 ZigBee SOC) will be released very soon, can I use CodeWarrior to work for it?

The ZigBee stack is open source?

 

Regards

Sam

ラベル(1)
0 件の賞賛
返信
1 解決策
2,152件の閲覧回数
tom_thompson
Contributor III

CodeWarrior will not be supporting the KW20 until the part goes into production.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,153件の閲覧回数
tom_thompson
Contributor III

CodeWarrior will not be supporting the KW20 until the part goes into production.

---Tom

0 件の賞賛
返信
2,152件の閲覧回数
connormosley
Contributor I

Will there be a special package of IAR EWARM offered which supports the KW20? Something similar to the EWARM-CM-FSL (which supports Kinetis K, L, and V series only).

Connor

0 件の賞賛
返信