Software tool for KW20 Family MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software tool for KW20 Family MCU

Jump to solution
2,284 Views
admin
Specialist II

The  KW20 MCU (Cortex4 ZigBee SOC) will be released very soon, can I use CodeWarrior to work for it?

The ZigBee stack is open source?

 

Regards

Sam

Labels (1)
0 Kudos
Reply
1 Solution
2,137 Views
tom_thompson
Contributor III

CodeWarrior will not be supporting the KW20 until the part goes into production.

---Tom

View solution in original post

0 Kudos
Reply
2 Replies
2,138 Views
tom_thompson
Contributor III

CodeWarrior will not be supporting the KW20 until the part goes into production.

---Tom

0 Kudos
Reply
2,137 Views
connormosley
Contributor I

Will there be a special package of IAR EWARM offered which supports the KW20? Something similar to the EWARM-CM-FSL (which supports Kinetis K, L, and V series only).

Connor

0 Kudos
Reply