Serial Interrupt Help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial Interrupt Help

跳至解决方案
3,445 次查看
LM
Contributor I

Serial Interrupt Help

Hi, I’m working on an MC9S12C32 (HCS12) and I’m having lots of trouble getting my program to accept inputs over the RS232 port.
I've loaded a program that drives a PWM and turns on an LED, and if it receives any data over the serial port it should turn off the LED.
Trying to communicate from my PC program to the serial port on the board wasn't working, so I actually put a signal on the receive pin of the J1 connector (PS0/RXD) and the LED properly turned off when it received the signal.

Is there anything odd like a jumper I have to remove or something to communicate to the board through the actual DB9 connector?

I tried switching the cable connecting the PC to the board with a null-modem cable instead, with still no success.

Any help would be greatly appreciated! :smileyhappy:

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,589 次查看
mke_et
Contributor IV
Uh, what board?  Did you design it?  Or are you talking one of the developement boards someone designed?
 
I used the 9S12 Badge from Future with the 9S12DP256 part on it and there are no jumpers for COM channel '0'.
 
 
 
 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,590 次查看
mke_et
Contributor IV
Uh, what board?  Did you design it?  Or are you talking one of the developement boards someone designed?
 
I used the 9S12 Badge from Future with the 9S12DP256 part on it and there are no jumpers for COM channel '0'.
 
 
 
 
0 项奖励
回复