RAM & FLASH Configurations in Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM & FLASH Configurations in Kinetis

ソリューションへジャンプ
1,642件の閲覧回数
punitkumar
Contributor IV

Hi,

i've seen two types of configurations for my project - RAM & FLASH.

I want to know

**What are the signifies?

*Which one if to be used & for what purpose?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,491件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

You can find some information to the link:

    RAM Target with Kinetis Design Studio and FRDM-K64F | MCU on Eclipse

RAM is using RAM memory whereas the FLASH is using FLASH memory too.

You can see the lcf file used is not the same.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,492件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

You can find some information to the link:

    RAM Target with Kinetis Design Studio and FRDM-K64F | MCU on Eclipse

RAM is using RAM memory whereas the FLASH is using FLASH memory too.

You can see the lcf file used is not the same.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信