RAM & FLASH Configurations in Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RAM & FLASH Configurations in Kinetis

跳至解决方案
1,681 次查看
punitkumar
Contributor IV

Hi,

i've seen two types of configurations for my project - RAM & FLASH.

I want to know

**What are the signifies?

*Which one if to be used & for what purpose?

标签 (1)
0 项奖励
回复
1 解答
1,530 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

You can find some information to the link:

    RAM Target with Kinetis Design Studio and FRDM-K64F | MCU on Eclipse

RAM is using RAM memory whereas the FLASH is using FLASH memory too.

You can see the lcf file used is not the same.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,531 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

You can find some information to the link:

    RAM Target with Kinetis Design Studio and FRDM-K64F | MCU on Eclipse

RAM is using RAM memory whereas the FLASH is using FLASH memory too.

You can see the lcf file used is not the same.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复