Pulse Train Simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pulse Train Simulation

Jump to solution
2,697 Views
tabull
Contributor I
    Hello -

I am using Full Chip Simulation of the 9S12C32 for part of my project development.  I want to measure the frequency of pulse signals from a Hall effect switch on a brushless DC motor to a port pin.  I have done this in the past using an MC68HC11F1.  I have now written code to do this using the 9S12, and I want to test the code first without a physical connection.

Is there a way to simulate such a series of pulses in Code Warrior Debugger Full Chip Simulation?  I have looked unsuccessfully for info on how one might do this.

Any help would be appreciated.

Thanks,
Dan

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,850 Views
imajeff
Contributor III
0 Kudos
Reply
1 Reply
1,850 Views
imajeff
Contributor III
0 Kudos
Reply