Pulse Train Simulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pulse Train Simulation

ソリューションへジャンプ
2,697件の閲覧回数
tabull
Contributor I
    Hello -

I am using Full Chip Simulation of the 9S12C32 for part of my project development.  I want to measure the frequency of pulse signals from a Hall effect switch on a brushless DC motor to a port pin.  I have done this in the past using an MC68HC11F1.  I have now written code to do this using the 9S12, and I want to test the code first without a physical connection.

Is there a way to simulate such a series of pulses in Code Warrior Debugger Full Chip Simulation?  I have looked unsuccessfully for info on how one might do this.

Any help would be appreciated.

Thanks,
Dan

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,850件の閲覧回数
imajeff
Contributor III
0 件の賞賛
返信
1 返信
1,850件の閲覧回数
imajeff
Contributor III
0 件の賞賛
返信