Watchpoint settin on a MC9S12NE64 using

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchpoint settin on a MC9S12NE64 using

Jump to solution
2,477 Views
AaronP
Contributor I
HI,
I'm trying to set a watch point on a MC9S12NE64 using V6.1 of the true time simulator with a P&E USB MULITLINK pod.  I disable all break points and set a watchpoing from the control points configuration window.  I hit the OK button and then go back into the control points window and there are no watchpoints set.  Can you set a watch point for this processor?  If so How do you do it?
 
Thank you for your help.
 
-AaronP
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,703 Views
CrasyCat
Specialist III
Hello
 
What are you trying to achieve here?
Where do you want to set your watchpoint?
Which steps are you performing to get it set?
 
Can you please be more specific?
 
Finally which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,704 Views
CrasyCat
Specialist III
Hello
 
What are you trying to achieve here?
Where do you want to set your watchpoint?
Which steps are you performing to get it set?
 
Can you please be more specific?
 
Finally which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 Kudos
Reply