MPC5675K Evaluation board Flexcan Demo Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5675K Evaluation board Flexcan Demo Code

Jump to solution
951 Views
barisiyidir
Contributor I


we are trying to send\receive can bus messages using 5675K Evaluation board. But we could not achieve to send\receive any can messages.

We are using 5675K (473 pin) in lock step mode. We are using the code given in "Example MPC5675K PinToggleStationery LSM CW210" for clock settings. Could anyone share demo flexcan code for 5675K Evaluation board.

 

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
798 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
799 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply