MPC5675K Evaluation board Flexcan Demo Code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5675K Evaluation board Flexcan Demo Code

跳至解决方案
1,557 次查看
barisiyidir
Contributor I


we are trying to send\receive can bus messages using 5675K Evaluation board. But we could not achieve to send\receive any can messages.

We are using 5675K (473 pin) in lock step mode. We are using the code given in "Example MPC5675K PinToggleStationery LSM CW210" for clock settings. Could anyone share demo flexcan code for 5675K Evaluation board.

 

Thank you.

标签 (1)
0 项奖励
回复
1 解答
1,403 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,404 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复