MPC5675K Evaluation board Flexcan Demo Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5675K Evaluation board Flexcan Demo Code

ソリューションへジャンプ
1,553件の閲覧回数
barisiyidir
Contributor I


we are trying to send\receive can bus messages using 5675K Evaluation board. But we could not achieve to send\receive any can messages.

We are using 5675K (473 pin) in lock step mode. We are using the code given in "Example MPC5675K PinToggleStationery LSM CW210" for clock settings. Could anyone share demo flexcan code for 5675K Evaluation board.

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,399件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,400件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Baris

Please refer to the attached example which does a simple communication between CAN_A and CAN_B modules on the EVB. The CAN_A is set to transmit a data and CAN_B then receive this data.

Hope it helps.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信