MPC5643L Interrupt vector table

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643L Interrupt vector table

ソリューションへジャンプ
3,223件の閲覧回数
olegivanus
Contributor III

Hi everyone.

I try to initialize LINflex module in MPC5643L to work in UART mode with interrupts, but cann't find information about how to organize interrupt handler for RX and TX events (how to init interrupt controller, what numbers/adresses of vectors for this events).

 

Maybe someone have example, which describes how to initialize interrupt controller and work in interrupt mode with UART?

Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,583件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Oleg,

Does the cookbook examples helped you to setup UART mode with interrupts?

MPC5643L UART examples

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,584件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Oleg,

Does the cookbook examples helped you to setup UART mode with interrupts?

MPC5643L UART examples

Stan

0 件の賞賛
返信
2,583件の閲覧回数
olegivanus
Contributor III

Hello, Stan. I can't understand, what DMA doing in this example.

It seems to be in this examples UART using software polling mode, DMA is initialized, but there are no handlers for DMA events such as "RX complete" or "TX complete".

I get for my project only baudrate and GPIO mode settings for UART.

Now I study how to using LINFLEX in UART mode using interrupts, because DMA mode is not yet acceptable for my application.

Thank for attention

10.04.2014, 14:46, "Stanislav Sliva" <[email protected]>:

MPC5643L Interrupt vector table

reply from Stanislav Sliva in CodeWarrior for MCU - View the full discussion

>

0 件の賞賛
返信