MWCT1xxx in CW10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MWCT1xxx in CW10.6

1,207 Views
bbosnjak
Contributor I

CW10.6 does not include support for MWCT1xxx MCUs. Is "CW MCU v10.5 Wireless Charging MWCT1xxx Service Pack" compatible with CW10.6?

Labels (1)
0 Kudos
Reply
4 Replies

638 Views
trytohelp
NXP Employee
NXP Employee

Hello Bernard,

Sorry for the delay.

I've contacted the product Manager and got the following details:

      - CW for MCU V10.6 is not supporting MWCT1xxx.

      - The CW MCU v10.5 patch for MWCT1xxx  is NOT compatible with CW MCU v10.6.

      - We are in the process of creating a CW MCU v10.6 service pack for MWCT1xxx.

      - We ran into some reference manual/register changes that we will address in the CW MCU v10.6 service pack.

      - Customers who need to develop with MWCT1xxx should stay on CW MCU v10.5 until the new service pack is available.


A patch should be released middle of may.

We recommend you to sign the newsletter

Go to the link:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

Click on Subscribe.


The patch will be posted on the web at link:

      http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_6


Regards

Pascal

0 Kudos
Reply

638 Views
Ben
Senior Contributor I

Pascal, please check and advise if CW10.6 support MC13234/7 chips (before installing it)

TIA

0 Kudos
Reply

638 Views
trytohelp
NXP Employee
NXP Employee

Hi Ben,

These processors are supported.

I've checked on my installation and I can select them under Project wizard.

Attached you will find the release note.

Perform a search for mc13.

Regards

Pascal

0 Kudos
Reply

638 Views
Ben
Senior Contributor I

Thank you Pascal for the answer. I just install it and saw what you mean.

I hoped that the new rev. has a full support for these chips, and that you embed the BeeKit automation in the CW10.6 PE

(as I have difficulty to activate project developed by BeeKit and CW10.5) but it is still not there.

Anyhow, 10.6 looks to be improved product for other chips too.

0 Kudos
Reply