MC9S09GT60 and CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S09GT60 and CodeWarrior

Jump to solution
2,540 Views
TaRaNTuLa
Contributor I
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!!



Many regards,Charis
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,458 Views
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

View solution in original post

0 Kudos
Reply
1 Reply
1,459 Views
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

0 Kudos
Reply