MC9S09GT60 and CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S09GT60 and CodeWarrior

ソリューションへジャンプ
2,530件の閲覧回数
TaRaNTuLa
Contributor I
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!!



Many regards,Charis
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,448件の閲覧回数
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,449件の閲覧回数
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

0 件の賞賛
返信