MC9S09GT60 and CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S09GT60 and CodeWarrior

跳至解决方案
1,993 次查看
TaRaNTuLa
Contributor I
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!!



Many regards,Charis
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
911 次查看
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

在原帖中查看解决方案

0 项奖励
回复
1 回复
912 次查看
peg
Senior Contributor IV


TaRaNTuLa wrote:
Hello guys!

I am a postgrad student and i have a project, concerning the MC13193 Evaluation Kit and its functions.

I want to use the X/Y/Z acceleration sensors of the SARD board(with MC13192 MCU), which is part of the MC13193 Evaluation Kit.When i choose "New Project" in CodeWarrior(ver. 5.7.0) and after a few "clicks" i have to select the suitable MCU for my project, i drop down the list of HCS08 Family and, unfortunately, there is nowhere the MC9S09GT60!There is only the MC9S08GT60, which is part of the EVB board.

Please help!!! :smileyhappy:



Many regards,Charis

Hi,

The MC13192 is the Zigbee radio NOT the MCU!

The SARD uses the MC9S08GT60!

There is no such thing as a 9S09GT60!

Hope that clears it up

Regards David


 

0 项奖励
回复