Key icon on .h file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Key icon on .h file

2,704件の閲覧回数
voider
Contributor II

I´m starting to use codewarior 10.x and I remove some files from the build to make some tests (click on the green mark) but when I enable again the key icon appears only on the .h file and I dont know what means.

Some one could help me to explain what is the icon and how can I remove it?

 

 

 

 

3401_3401.pngpastedImage_0.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,421件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi,

The KEY icon shows that the file has other settings than the rest of the project that it belongs too. For example the project might have debug information enable while the file has this disabled.

This is a simple way to check if all your files inherits the projects settings.

To get rig of it you need to right click on that file then select /Resource Configuration/Reset to Default

1.png

Hope this helps!

0 件の賞賛
返信

2,421件の閲覧回数
voider
Contributor II

But for .h files this option is not in the menu.

3413_3413.png

0 件の賞賛
返信

2,419件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

I use CW10.6.4, this option exists on my side for .h file.

see my video attached.

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信