Key icon on .h file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Key icon on .h file

3,645 次查看
voider
Contributor II

I´m starting to use codewarior 10.x and I remove some files from the build to make some tests (click on the green mark) but when I enable again the key icon appears only on the .h file and I dont know what means.

Some one could help me to explain what is the icon and how can I remove it?

 

 

 

 

3401_3401.pngpastedImage_0.png

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

3,362 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi,

The KEY icon shows that the file has other settings than the rest of the project that it belongs too. For example the project might have debug information enable while the file has this disabled.

This is a simple way to check if all your files inherits the projects settings.

To get rig of it you need to right click on that file then select /Resource Configuration/Reset to Default

1.png

Hope this helps!

0 项奖励
回复

3,362 次查看
voider
Contributor II

But for .h files this option is not in the menu.

3413_3413.png

0 项奖励
回复

3,360 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

I use CW10.6.4, this option exists on my side for .h file.

see my video attached.

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复