ICS custom trim on CW 6.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ICS custom trim on CW 6.1

跳至解决方案
2,426 次查看
fabio
Contributor IV
Hi,

Did anybody noticed any problem with the trim customizing feature of CW6.1?

Using CW6.0 I could set the desired ICS frequency and the NV_FTRIM and NV_ICSTRM were programmed accordingly.

Using CW6.1 I set the desired frequency for the ICS internal reference but it appears that this custom frequency is not read by CW. The debugger/BDM keeps setting the ICS to the default 16MHz operation.

Is this only happening to me?

Best regards,


Message Edited by fabio on 2008-03-14 05:02 PM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,286 次查看
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,286 次查看
Klined
Contributor I
Hi,

I can say you are not the only one experiencing this.  I have noticed the same behavior when I upgraded from CW 6.0 to 6.1, and I'll say it's quite annoying.  For those situations requiring correct custom trim, I still use CW 6.0.  I hope they fix this in CW 6.1 or the next release.

0 项奖励
回复
1,286 次查看
J2MEJediMaster
Specialist I
I am looking into this.

---Tom
0 项奖励
回复
1,287 次查看
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom
0 项奖励
回复