ICS custom trim on CW 6.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICS custom trim on CW 6.1

Jump to solution
2,511 Views
fabio
Contributor IV
Hi,

Did anybody noticed any problem with the trim customizing feature of CW6.1?

Using CW6.0 I could set the desired ICS frequency and the NV_FTRIM and NV_ICSTRM were programmed accordingly.

Using CW6.1 I set the desired frequency for the ICS internal reference but it appears that this custom frequency is not read by CW. The debugger/BDM keeps setting the ICS to the default 16MHz operation.

Is this only happening to me?

Best regards,


Message Edited by fabio on 2008-03-14 05:02 PM
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,371 Views
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom

View solution in original post

0 Kudos
Reply
3 Replies
1,371 Views
Klined
Contributor I
Hi,

I can say you are not the only one experiencing this.  I have noticed the same behavior when I upgraded from CW 6.0 to 6.1, and I'll say it's quite annoying.  For those situations requiring correct custom trim, I still use CW 6.0.  I hope they fix this in CW 6.1 or the next release.

0 Kudos
Reply
1,371 Views
J2MEJediMaster
Specialist I
I am looking into this.

---Tom
0 Kudos
Reply
1,372 Views
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom
0 Kudos
Reply