How to program DSP56F805F?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program DSP56F805F?

1,044 Views
khengwahtan
Contributor I


Please help to provide CW software step by step to program .elf file into DSP56F805F.

Labels (1)
0 Kudos
Reply
1 Reply

998 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello

Do you have CodeWarrior project for the ELF file? If yes, just open the project and click on the ‘debug’ icon to program the target. If you only have ELF file without project, please refer to the section ‘Debugger for 56800E-> Loading .elf File without Project’ in 56800E Targeting Manual:

C:\program files\Freescale\CodeWarrior for DSC56800E v8.3\Help\PDF\Targeting_56800E_cd.pdf

Hope this helps!

 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply